LPCXpresso5411X LQFP64 REV A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso5411X LQFP64 REV A

2,190件の閲覧回数
santoshganachar
Contributor II

hi 

how to flash hex file LPCXpresso 54114 eval board, i'm trying flash hex file with "Flash magic Tool" getting some Error "auto Boud" can you help me any other open source flashing tool.

0 件の賞賛
返信
3 返答(返信)

1,992件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

In order to use the Flash magic Tool for the  LPCXpresso 54114 eval board, please check the following steps:

1. Unplug the USB cable (if attached). 

2. Press and hold the ISP0 SW2 button.

3. Plug in a USB cable from a USB computer to the J7 (“Link”).

4. Release the SP0 SW2 button.

5. Open Flash magic Tool

6. Select the device and the COM port.

pastedImage_1.png

The COM Port depends on the Communications Port of your Computer's RS232. When you use this COM Port with FlashMagic – be sure that no other program is using it at this time.

You can check the COM port using the device manager >Ports (COM & LPT)

pastedImage_5.png

7. If you want to check if FlashMagic is working with your board use the "Read Device Signature" option:

pastedImage_6.png 

If everything is ok you will see this window with your device ID on it.

pastedImage_7.png

I hope this helps,


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,992件の閲覧回数
santoshganachar
Contributor II

thanks very much

then next step what will do

0 件の賞賛
返信

1,992件の閲覧回数
santoshganachar
Contributor II

Thanks

It's Working.

0 件の賞賛
返信