LPCXpresso with MCB1700 (and KEIL ULINK-ME)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso with MCB1700 (and KEIL ULINK-ME)

955 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mandar_Pitale on Wed Feb 20 16:42:52 MST 2013
Hello,

Currently I am have the MCB1700 board with LPC1769FBD100. I also have KEIL-ULINK ME.

I had created a sample project usinf LPCXpresso and tried to download/debug my application but it complains that "No Compatible Emulators available".

I am not too sure if I had done something wrong or in principle its not possible to use the LPCXpresso with MCB1700 via KEIL-ULINK ME.

Kindly suggest.

Regards,
Mandar
标签 (1)
0 项奖励
回复
1 回复

874 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Feb 20 17:57:03 MST 2013
LPCXpresso Download / Debug function is using LPC-Link or Red Probe.