LPCScrypt and Keil ULINK2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCScrypt and Keil ULINK2

2,065件の閲覧回数
enzofaffa
Contributor I

Hello, is it possible to program an ARM LPC43S3X by a ULINK2 programmer using the JTAG interface by means of LPCScrypt?

I managed to perform a programming by command line with the "crt_emu_cm_redlink" tool and ULINK2, but I'm looking for a n alternative stand-alone tool (I don't want to have LPCXpresso installed)

TY

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,906件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

No - LPCScrypt communicates with the target using VCOM over USB.  If your target board support DFU boot, then LPCScrypt can boot and program any internal flash devices or a Supported SPIFI flash.

This is fully described in the LPCScrypt documentation.

Yours,

LPCXpresso Support

0 件の賞賛
返信

1,906件の閲覧回数
enzofaffa
Contributor I

Thank you.

I obviously read the documentation and spent time to try to understand, but I was a bit confusing about USB...in my mind it was the USB communication between host PC and ULINK2, so my post to this forum.

Now I definitely understand that USB you're talking about is a way to access the MCU itself (that is, alternative to JTAG).

Do you have any clue about a tool different than LPCScrypt to achieve my needing? 

Thanks again and in advantage

Enzo

0 件の賞賛
返信