LPCOpen project files for LPC1549 Motor Control Kit (BLDC)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCOpen project files for LPC1549 Motor Control Kit (BLDC)

1,391 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ChrisHill on Thu Aug 14 01:32:18 MST 2014
Hello,

I have one of the LPC1549 Motor Control Kits (BLDC) Product # OM13068. Two questions:


1) Are the latest LPCOpen project files the ones found at this link?

http://www.nxp.com/documents/application_note/AN11523.zip

If not - where would I find them?


2) From searching this forum, I understand that there is no GUI for the BLDC version (only PMSM). Is this still true?


Thanks and regards...

Chris.
标签 (1)
0 项奖励
回复
1 回复

1,357 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Aug 14 10:54:24 MST 2014
Hi ChrisHill,
At this moment there is no LPCOpen project for this BLDC motor control example.
Also right now, there is no GUI for this BLDC motor control example.
0 项奖励
回复