LPCExpresso 7.8 with LPC15xx 2.08c library, no CMSIS within CMSIS_CORE library....

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCExpresso 7.8 with LPC15xx 2.08c library, no CMSIS within CMSIS_CORE library....

967件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by riscy00 on Wed Jul 15 12:07:21 MST 2015
Hi

I have used LPC17xx and LPC8xx and LPC11Uxx which includes CMSIS.

I now notice there is no CMSIS for LPX15xx and that left me tad concern. (within C:\nxp\LPCXpresso_7.8.0_426\lpcxpresso\Examples\CMSIS_CORE)

I looked into NXP website but could not understand meaning of "superset of LPCOpen". What happen and why it decided to move on to make CMSIS invisible.

I do not wish to use board library since that applies to eval board, but can use chip library and make my own custom app and board . Am I corrects to assumed the CMSIS are build in chip library?

Thank in advance for quick reply.

R.
ラベル(1)
0 件の賞賛
返信
1 返信

944件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 16 00:16:22 MST 2015
We no longer provide standalone CMSIS library projects for newer MCUs (basically those released in the last 2 years or so). The functionality of the old CMSIS library projects (which basically means the Cortex-M core and MCU peripheral header files) has basically been merged into our LPCOpen product, which also adds in peripheral drivers.

When using LPCXpresso IDE to produce an LPCOpen-based project, you can either select LPCOpen chip and board libraries to link against, or just the appropriate chip library. Please read the LPCXpresso User Guide (and watch the video at  http://www.lpcware.com/lpcxpresso) for more details

More information on LPCOpen together with package downloads can be found at: http://www.lpcware.com/lpcopen

Regards,
LPCXpresso Support
0 件の賞賛
返信