[LPC8xx] SPI ROM driver, missing DMA_HANDLE_T specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LPC8xx] SPI ROM driver, missing DMA_HANDLE_T specification

1,832件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pgr on Wed Dec 02 01:56:32 MST 2015
Dear all,

I am currently adding support for the SPI ROM driver in LPCOpen for theLPC8xx.
The definition of type DMA_HANDLE_T is missing in the user manual.

Does anyone can please give me the correct specifications of this type ?

Any reason why ROM SPI driver is the only driver missing from LPCOpen ?

Regards
PGR
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,798件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pgr on Thu Dec 03 00:48:20 MST 2015
Why ?
0 件の賞賛
返信

1,798件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Thu Dec 03 00:15:00 MST 2015
Hi PGR,

I did not get a chance to check yet, but my guess void * for the type of DMA_HANDLE_T.
The SPI ROM driver in general (especially the slave driver) is not recommended for use.

Best regards,
-NXP Support
0 件の賞賛
返信