LPC845 DAC1 Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC845 DAC1 Configuration

ソリューションへジャンプ
2,526件の閲覧回数
kk7xo
Contributor III

I am using the LPCXpresso845-MAX board and wish to use DAC1 which is connected to the speaker.  In the schematic for the board it shows that the speaker is connected to DAC1 via pin PIO0_29. 

Referring to the LPC845 user manual UM11029 rev 1.7 of April 2021 I see that in the IOCON register for DAC0, PIO0_17, there is a DACMODE bit (number 16) that must be set to use DAC0, but in IOCON register for PIO0_29 there is no corresponding bit for DAC1. 

How do I set DACMODE for DAC1 in PIO0_29?

 

0 件の賞賛
返信
1 解決策
2,514件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @kk7xo 

There isn't this bit, no need config DACMODE bit.

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,514件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @kk7xo 

There isn't this bit, no need config DACMODE bit.

 

BR

Alice

0 件の賞賛
返信
2,500件の閲覧回数
kk7xo
Contributor III
Thank you!
0 件の賞賛
返信