LPC824 TSSOP WKTCLKIN pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC824 TSSOP WKTCLKIN pin

962件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by joepbrown on Mon Mar 23 23:18:07 MST 2015
Am I correct in reading the LPC824 datasheet that the WKTCLKIN pin in unavailable on the TSSOP package?

This would also infer that there is no way use an external clock in deep-power-down mode on the TSSOP package...which means the only option for the clock in deep-power-down on the TSSOP is the sloppy 10khz low-power oscillator and there's really no way to maintain decent timing and use the deep-power-down mode (like an RTC).
ラベル(1)
0 件の賞賛
返信
1 返信

928件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Mon Apr 27 22:47:44 MST 2015
Hi,
Your understanding is correct. UM Section 6.3.1 has a "Remark" on this clarification:
The external clock input WKTCLKIN on the wake up timer is not available on the TSSOP20 package.
Regards,
0 件の賞賛
返信