LPC824 SPI Sample Code with MCUXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC824 SPI Sample Code with MCUXpresso

2,258件の閲覧回数
ellenlin
Contributor III

Now i am using LPC824 Demo_Example from SDK_2.4.2_LPCXpresso824MAX .

But i don't understand how to realize the demo_example . Following is all example i wanna know , 

  

How to setting the EVM ? What tools i have to use it ? thanks !!

pastedImage_1.png

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,985件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Select all spi examples and click Finish in order to import to the workspace.

pastedImage_1.png

After do that, you can find a readme document under doc folder that you can use as reference.

pastedImage_2.png

I hope this helps,

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,985件の閲覧回数
ellenlin
Contributor III

Dear Soledad , 

   i has already download 2 evm with SPI_Interrupt_Master ( Debug Mode ) & SPI_Interrupt_Slave ( Free RUN )

   but transfer date fail , what is happening ? 

   i need you suggestion to solve this and i can keep going my application , thanks a lot !! 

pastedImage_1.png

0 件の賞賛
返信