LPC824: PWM in sleep/power-down mode possible?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC824: PWM in sleep/power-down mode possible?

跳至解决方案
1,763 次查看
robin_maeder
Contributor II

On the LPC824 I need a pin with a PWM signal while the current consumption is as low as possible. So which is the lowest power mode where I can ouptut a PWM to a pin? 

标签 (1)
0 项奖励
回复
1 解答
1,744 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Robin,

I think the PWM signal can continue to output PWM signal for the SCTimer/PWM module in sleep mode. In sleep mode, only the core stop working.

As the following figure, digital peripherals can continue to work in sleep mode.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,745 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Robin,

I think the PWM signal can continue to output PWM signal for the SCTimer/PWM module in sleep mode. In sleep mode, only the core stop working.

As the following figure, digital peripherals can continue to work in sleep mode.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 项奖励
回复