LPC824 IAP routines do not work on common comand/result buffer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC824 IAP routines do not work on common comand/result buffer

1,770 Views
wernerf
Contributor II

Hi all,

working on an LPC824 project I re-used the IAP routines of an older LPC1768 project which worked fine there. These IAP routines use a common buffer for both command input and result output. The user manual explicitely allows this to be done.

pastedImage_4.png

Unfortunately this doesnt work with the LPC824 (at least Rev. 1A). You will always get an INVALID_COMMAND code as result. It looks like the IAP routine writes to ComRes[0] too soon an kills its own command.

So the user manual (UM10800) is wrong here and you HAVE TO use two different buffers.

pastedImage_3.png

Labels (1)
0 Kudos
Reply
1 Reply

1,514 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Werner Fritsch,

I'd like to suggest that you can refer to the flashiap demo in the LPCOpen, and the demo demonstrates programming a FLASH block during run-time and generating a FLASH signature.

The LPCOpen's link:

cache.nxp.com/files/microcontrollers/software/LPCWare/lpcopen_2_19_keil_iar_nxp_lpcxpresso_824.zip

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply