LPC824 Glitch Filter Clock Divide Register Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC824 Glitch Filter Clock Divide Register Issue

1,206件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by efiLabs on Sat Nov 15 18:37:29 MST 2014
there is already a slightly similar post on the 812, but i want to elaborate on the 824

to set a glitch filter a few things need to happen

1) in order to write to the iocon regs the peripheral clock to the iocon block needs to be enabled

/* Enable the clock to the IOCon Block */
  Chip_Clock_EnablePeriphClock (SYSCTL_CLOCK_IOCON) ;

2) set the S_MODE (sample mode) bits to the desired IOCONFILTR_PCLK) count

  Chip_IOCON_PinSetSampleMode (LPC_IOCON, IOCON_PIO15, PIN_SMODE_CYC3) ;

3) set the desired IOCON glitch filter clock divider registers 6 to 0 (IOCONFILTCLKDIVx) to the desired IOCONFILTR_PCLK ... please observe the numbering of 6 to 0

  Chip_IOCON_PinSetClockDivisor (LPC_IOCON, IOCON_PIO15, IOCONCLKDIV0) ;

4) now that the iocon regs are set the peripheral clock can be turned off again

/* Disable the clock to the IOCon Block */
  Chip_Clock_DisablePeriphClock (SYSCTL_CLOCK_IOCON) ;

5) and this is the tricky part now ... remember that the IOCONFILTCLKDIVx regs are in descending order of 6 to 0 (outlined in item 3)

  LPC_SYSCTL->IOCONCLKDIV[6] = 0x00ff ;/* IoConClkDiv - 0 = div 255*/

IOCONCLKDIV[6] is IOCON glitch filter clock divider register 0 and NOT 6

6) note that "typedef enum CHIP_PIN_CLKDIV { ..." can only be used for setting the IOCON clock divisor field bits 15 - 13 in the PIO0_xx regs
and can NOT be used as index into the 7 IOCONCLKDIV[index] regs

i wish there would be an enum for the indexing in the 7 IOCONCLKDIV[x] regs to really show this reverse order of reg index vs reg number


7) on top of it if you try to look at the IOCONCLKDIV[x] regs in xpresso, all you see is IOCONCLKDIV6 and no 5 - 0 ... maybe the xpresso guys will read this and try to fix it in the next revision

cheers efiLabs

ラベル(1)
0 件の賞賛
返信
1 返信

1,099件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jgoulder on Wed Jan 21 07:34:18 MST 2015
I have been diving into LPC8xx.h and noticed this as well.  It seems very confusing when you set IOCONCLKDIV[0] and it is really setting the IOCONCLKDIV6 register.

I think it should be defined in the header file individually as:

   ...
   __IO uint32_t IOCONCLKDIV6;
   __IO uint32_t IOCONCLKDIV5;
   __IO uint32_t IOCONCLKDIV4;
   __IO uint32_t IOCONCLKDIV3;
   __IO uint32_t IOCONCLKDIV2;
   __IO uint32_t IOCONCLKDIV1;
   __IO uint32_t IOCONCLKDIV0;
   ...

instead of using an array.

0 件の賞賛
返信