LPC812+ lpclink2+keil can download program but cannot execute

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC812+ lpclink2+keil can download program but cannot execute

1,851件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ramniraj10 on Tue Apr 28 11:20:20 MST 2015
After running program for 5 days, t suddenly stopped.
When connected  to debugger, it can download code but cannot start debugging(cannot access memory)
Earlier it was working fine with same set up and configuration.

When i checked each of the pin of LPC812, found 2 pins are at 0 volt(PIO0_12 and PIO0_7) while other pins where at high voltage(3.3V).

Can you suggest what might be the issue?

Thanks,
Niraj Ram
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,789件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ramniraj10 on Wed Apr 29 02:14:11 MST 2015
One more thing, ISP pin(PIO0_12) is always low when checked teh signal using oscilloscope.
No pins are shorted among each other.

Thanks,
Niraj Ram
0 件の賞賛
返信

1,789件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ramniraj10 on Wed Apr 29 02:12:19 MST 2015
Dear whitecoe,

ISP mode is needed when the debugger cannot access debug port(cannot connect to device) and also cannot download code in to flash.
In my case, I can download code into flash but cannot start debug access.

When start any debug session, program runs automatically but I cannot see any breakpoint or memory.
Debugger always pop up "cannot access memory" all the time.

Cannot jump to reste vector or function main().

Thanks,
Niraj Ram

0 件の賞賛
返信

1,789件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Wed Apr 29 00:21:01 MST 2015
Try booting into ISP? http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

HTH!
0 件の賞賛
返信