LPC804 Writing into Flash memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC804 Writing into Flash memory

ソリューションへジャンプ
3,562件の閲覧回数
ashokfair
Contributor IV

Hi Everyone,

Im currently using the SDK Version: KSDK 2.4.1 (2018-06-18) for LPC804 ,

Please help me to write data in Flash memory , im not finding any example for the same.

Thanks,

Ashok

ラベル(1)
0 件の賞賛
返信
1 解決策
3,321件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Ashok Ra,

Here is an example for writing in flash memory for the LPC802, it should work in the LPC804 too.

Hope it helps,

Alexis Andalon

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,321件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Ashok Ra,

Here is an example for writing in flash memory for the LPC802, it should work in the LPC804 too.

Hope it helps,

Alexis Andalon

0 件の賞賛
返信
3,321件の閲覧回数
ashokfair
Contributor IV

Hi Alexis,

Thank you so much. I tested the code with LPC804 and working fine and verified OK  :smileyhappy:

pastedImage_3.png

Thanks,

Ashok R

0 件の賞賛
返信
2,674件の閲覧回数
BerlinRaj
Contributor II

dear ashok, can you please post how to read the value from the flash memory ?

0 件の賞賛
返信