LPC55xx API

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55xx API

526 Views
Lor75
Contributor I

Hello,

for a new project I want to use LPC550x microcontroller with IAR Embedded Workbench: in the past I have used other LPC MCU (LPC1317, LPC1788, LPC1788)

Now i read everywhere that some functions can be managed only by using API but I don't understand how to use them; are these function available only with MCUXPRESSO?

I would like to avoid API and write my own code but I don't fine the C code of these API. For example CAP BANK for oscillators are only documented with API so if I don't use API I can't use these CAP BANK. Is it correct?

I have a big confusion in my mind about this.

Can anyone help me? It's for my job

Best regards.

0 Kudos
Reply
2 Replies

320 Views
kipoke3113
Contributor I

Hello,

Just like your past LPC microcontrollers, the LPC550x is a standard memory-mapped architecture. You are never forced to use NXP's driver APIs. You can write pure, direct-register C code using standard CMSIS header files (lpc55s06.h, etc.) provided by IAR or NXP.


Best Regards

0 Kudos
Reply

495 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Lor75 

For newer NXP MCUs, including the LPC55xx series, we recommend using the MCUXpresso SDK drivers, which include both APIs and source code.

You can download the SDK from:

https://mcuxpresso.nxp.com/builder?hw=LPCXpresso55S06&rel=943 

For detailed instructions, please refer to:

https://www.nxp.com/document/guide/getting-started-with-the-lpc55s06-evk-evaluation-board:GS-LPC55S0...  

Additionally, the LPC55xx series is supported by MCUXpresso IDE, which is free to use with no restrictions on functionality or code size.

You can download MCUXpresso IDE from:

https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools... 

 

If still have any question, please feel free to contact me. Thank you. 

BR

Alice

0 Kudos
Reply