LPC55s28 PN5190 NFC Read Library porting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55s28 PN5190 NFC Read Library porting

64 Views
RadoslawTomasik
Contributor I

Hello Community,
hello NXP-Team

I'm looking for LPC55S28 ↔ PN5190 connection details (Host SW + DAL / BAL layer)

I already have the PN5190 NFC Reader Library and would like to connect the LPC55S28 MCU to the PN5190 NFC frontend.

I have reviewed the article “Using NFC Reader Library with LPC55S69”, but I am looking specifically for an LPC55S28‑compatible setup.

Questions

  1. Is there an existing DAL/BAL (Driver Abstraction Layer) implementation for connecting the LPC55S28 to the PN5190?
  2. Has anyone successfully connected LPC55xx (LPC55S16 / LPC55S28 / LPC55S69) to a PN5190 using the NFC Reader Library?
  3. Is there a ready solution, reference project, or recommended starting point for the LPC55S28 + PN5190 combination?
  4. If not, is the LPC55S69 guide the correct and closest reference to follow for porting?

Thank you!




0 Kudos
Reply
1 Reply

1 View
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @RadoslawTomasik

My apologies, there is no specific documentation or guide for PN5190 + LPC55S28.

However, as you mention, you can refer to the following guides:

- Using NFC Reader Library with LPC55S69

- NFC Reader Library Porting FRDM_K64F

- NFC Reader Library Porting to i.MX RT1050 - NXP Community

Those guides can be a good starting point.

Regards,
Eduardo.

0 Kudos
Reply