LPC55S6x for low power application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S6x for low power application

1,430件の閲覧回数
RamKoppu
Contributor I

Is it possible to make one of the M33 cores as always ON and wake up the another M33 explicitly on demand when higher processing is required? Is there any example code for this low power use case for LPC55S6x?

0 件の賞賛
返信
1 返信

1,419件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

The dual core in the LPC55xx/LPC55Sxx is asymmetric architecture, which means one core (CPU0) is a master one and the other (CPU1) is a slave one. The CPU0 is factory set to the master which can work normally and the CPU1, slave core, is on hold and its clock is disabled with the chip startup. To let it work, the slave core needs to be released and its clock can be enabled through a register by the master core.

So you can make CPU0 always on, enable CPU1 clock if needed. Sorry there isn't exactly example, while there is dual core demo under SDK, and there is an Application note, you can configure it how to enable CPU1:
https://www.nxp.com.cn/docs/en/application-note/AN12358.pdf  

 

BR

Alice

0 件の賞賛
返信