LPC55S69JEV98

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69JEV98

947 Views
tejas_Kt2i
Contributor I

Currently we are developing a product that requires sleep mode, and the controller itself is consuming 1.1mA but when we remove the power only for VDD pins, the functionality is still working, and the current consumption is dropped to 0.15 mA. 

This scenario we have seen in 2 boards out of 3 boards. where the 3rd board functionality itself failed when we removed the VDD connection

Attached the schematics snap

tejas_Kt2i_0-1748503791709.png

 

0 Kudos
Reply
1 Reply

885 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @tejas_Kt2i 

 

  1. Do you mean that two  boards have issues when the VDD power is removed?
  2. Regarding "the third board failed when the VDD connection was removed": Please point out which specific functions failed.
  3. Note: VDD is the power supply for the I/Os.
  4. Please share the schematic in PDF format.

 

 

BR

Alice

 

0 Kudos
Reply