LPC55S69 : SDK2.8.2 vs 2.8.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : SDK2.8.2 vs 2.8.0

2,769件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

I can see SDK2.8.2 revert back clock drivers fsl_clock.c/h from version 2.3.3 to 2.3.2.

Also all versions of powerlib are updated.

What was problems with previous version of powerlib and should I take versions from 2.8.2 SDK ?

Or it can be other corrections ?

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,734件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

This should be a typo. I will let you know once I get feedback from SDK development team.

0 件の賞賛
返信

2,712件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

By checking, SDK2.8.0 fixes the defect of KPSDK-35743 but SDK2.8.2 not. 

fix of KPSDK-35743 is attached.

To summarize

  • 2.8.0 includes fix , so  fsl_clock.c/h version is 2.3.3
  • 2.8.2 contains bug ( s_Pll0_Freq is incorrect), so fsl_clock.c/h version is 2.3.2

The problem is 2.8.2 and 2.8.0 are executed at the same time, so there is some synchronize issue. The release workflow will be refined to avoid the confusion.

 

Have a nice day,

Jun Zhang

0 件の賞賛
返信