LPC55S69 : SB2.1 max size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : SB2.1 max size

2,011件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

LPC55S69 have 640KB of flash memory and 320KB of SRAM.

I have plan to update at list 512KB of flash memory and use SB2.1 container for keep update. ( Secure boot in use.)

I assume that SB2.1 loaded to SRAM, signature is verified and only after that existing flash memory is erased 

and new firmware flashed from SRAM to Flash.

But we have only 320 KB of SRAM and romcode use some part as well.

How it is really works ?

Should I cook several SB2.1 files and use those one by one and do not reboot in between ?

How update 512KB of firmware in secure way with help of SB2.1  container ?

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,936件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eugene,

When update,  SRAM only receive a part of data for authentication , not all of them,

if passed, continue receive. so 320K RAM is enough.

Hope it helps,

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,936件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi Alice_Yang‌ !

Can you explain more details.

What exact part of file are authenticated ?

Does erase is done immediately after that ?

After that data from ISP just encrypted and written in flash on block basis ?

Can any update to be splitted for several SB2.1 files. Each file can cover some flash address range.

If sudden power loss is happens during SB2.1, I hope update is possible to restart again without any problem ?

Regards,'Eugene

0 件の賞賛
返信

1,936件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eugene,
About the detail , please refer to the Elftosb user manual, especially the
Chapter 6 Appendix B: SB boot image file format.

https://www.nxp.com/docs/en/user-guide/MBOOTELFTOSBUG.pdf   

Hope it helps,

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信