LPC55S69-EVK Simultaneous USB Host and Device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69-EVK Simultaneous USB Host and Device

1,534件の閲覧回数
ja2022
Contributor I

Hello,

I have a question about this dev board and this microcontroller. What I would like to do, is have both a USB device and a USB host on one microcontroller, acting as a "proxy" for the USB device connected to the board.

The user manual mentions that either port can be configured as a host at once in section 6.1, but nothing on using one as a host and one as a device. Is this a possible thing to do with this platform? If not, where else should I look within NXP microcontrollers?

Thank you!

ラベル(1)
0 件の賞賛
返信
1 返信

1,518件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

Yes you can have both a USB device and a USB host on one microcontroller.

I suggest you setting different task priority on each task when created. You could take keyboard2mouse sdk example as reference.

Hope this helps,

Jun Zhang

0 件の賞賛
返信