LPC55S66 : wakeup reason

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S66 : wakeup reason

2,597 Views
EugeneHiihtaja
Senior Contributor I

Hi !

Is any fast way exists to know wakeup reason when CPU exit from API POWER_EnterPowerDown() ?

Some power API ?

Or we should analyze pending interrupts from list of uint64_t wakeup_interrupts what were specified ?

Regards,

Eugene

Labels (1)
0 Kudos
Reply
3 Replies

2,498 Views
soledad
NXP Employee
NXP Employee

Hi,

Like you mentioned you should analyze pending interrupts in order to know what was.

Regards

Soledad

0 Kudos
Reply

2,497 Views
EugeneHiihtaja
Senior Contributor I

Hi soledad‌ !

I'm using POWER_EnterPowerDown()  on secure side and it called from nonsecure RTOS scheduler hook.

Nonsecure interrupts are disabled but secure not.

GIntx interrupts processed on secure side and when I have exit after POWER_EnterPowerDown(), GINTx

already occurs after 343us ( like in spec) but exit happens after 450 us and GINTx is not pending any more.

It means I should disale all interrupts and they will be not processed so fast as expected.

may be some POWER API can remember reason of last exit ?

Regards,

Eugene

0 Kudos
Reply

2,497 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hello, Eugene,

Unfortunately, none of the  fslpower power functions, from fslpower API  is capable to retrieve the wake-up source.

Best regards, Diego. 

0 Kudos
Reply