LPC55S36 EVK board: CMSIS-DAP Update causes "No connection to chips debug port"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S36 EVK board: CMSIS-DAP Update causes "No connection to chips debug port"

5,756 Views
brandonProgramming
Contributor I

I am working on an LPC5536 EVK board and was able to run the example code. I then updated the CMSIS-DAP firmware from 2.245 to 3.133 and now I receive the following error messages when I attempt to debug my example software program "led_blinky".

I am using MCUXpresso 11.9

Labels (2)
0 Kudos
Reply
4 Replies

5,729 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @brandonProgramming 

I don't think problem is CMSIS-DAP firmware  3.133. I test this firmware with LPC55s36-evk, there is no issue. While I have MCU-LINK_installer_2.250.exe, you can test if need. Can not find 2.245.

Recommend you enter ISP mode, then use GUI Flash tool inside MCUXpresso IDE (or blhost tool)  erase flash all. then Remove ISP jumpers. Create a new IDE workspace, import LED demo. Debug again.

Alice_Yang_0-1709625125416.png

 

BR

Alice

 

 

0 Kudos
Reply

5,712 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @brandonProgramming 

Enter ISP mode through connecting 3-4 of J43.

Alice_Yang_0-1709688335567.png

 

BR

Alice

 

0 Kudos
Reply

5,719 Views
brandonProgramming
Contributor I

I gave the GUI flash tool a try to erase all flash, but there are no probes for me to connect to...Note the board was in isp mode by shorting out J25.

brandonProgramming_0-1709644607116.png

 

0 Kudos
Reply

5,754 Views
brandonProgramming
Contributor I
Does anyone have CMSIS-DAP MCU-LINK_Installer_2.245
0 Kudos
Reply