LPC55S28 UART RX IDLE INTERRUPT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S28 UART RX IDLE INTERRUPT

1,014 Views
playbear
Junior Contributor I

Hello,NXP!

 I'm using LPC55S28 in my project,and I find that LPC55S28 DO NOT SUPPORT uart rx idle interrupt or Character Time-out Indicator (CTI) like LPC1768???

 for example , if I set 15 to rx fifo trig level , I send only 1 bytes to LPC55S28, how do I know there is 1 byte data in rx fifo?No way to notice/trig user application to know there is 1 byte in rx fifo?What I can do is polling the fifo stat all the time?

Please help me, give me some better ideas?Thank you.

Labels (1)
0 Kudos
Reply
1 Reply

992 Views
danielholala
Senior Contributor II

With LPC55xx having no support for RX TIMEOUT, you are best of with reading single bytes only. I'm successfully using USART_TransferReceiveNonBlocking() requesting only 1 byte at at time. 

0 Kudos
Reply