LPC55S26JEV98 || Power Supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S26JEV98 || Power Supply

1,511 Views
JyotiVaishnav
Contributor II

Hello Team, 

We are using an LPC55S26JEV98 processor in our design. 

Following below mentioned connections we did in our design for power rails.  
VDD_1 / VDD_2 / VDD_3 / VDD_4 - are connecting to 1V8 
VDD_PMU / VDDA / VBAT_DCDC / VBAT_PMU - are connecting to 3V3 

We want to know that there is any problem or issue to connect VDD_PMU / VDDA / VBAT_DCDC / VBAT_PMU the mention supplies to 3V3 voltage level. 

 

Labels (1)
0 Kudos
Reply
2 Replies

1,474 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As TwoBias said, for the VDD_PMU power supply pin, we suggest you use internal DC/DC converter for the VDD_PMU power supply as the following Fig. The VDD_PMU power supply input voltage is from 1.1V to 1.2V, which can be controlled with software based on the core frequency.

It is okay that

VDD_1 / VDD_2 / VDD_3 / VDD_4 - are connecting to 1V8 
VDDA / VBAT_DCDC / VBAT_PMU - are connecting to 3V3 

Hope it is helpful

xiangjun_rong_0-1691462102615.png

BR

XiangJun Rong

 

0 Kudos
Reply

1,489 Views
TwoBias
Contributor II

Hi,

you should not connect VDD_PMU to 3,3V.

It is core supply and maximum voltage is 1,26V.

You should connect it with the DCDC output path and FB Pin.

BR

 

0 Kudos
Reply