LPC55S16 MCAN PSR Functions question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S16 MCAN PSR Functions question

3,498 Views
jmorel
Contributor II

for my project I'm trying to utilize the register to better control the mcan module how i need and i see this PSR ACT portion give me part of what I'm looking to do, but it doesn't seem to work as stated in the Manuel. when testing I'm not seeing ACT change and always indicates idle. how is the ACT portion of the PSR suppose to work?

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

3,479 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As the name of PSR implies, the ACT bits reflect the state of CAN bus, if you want to see if the ACT bits change or not based on CAN bus action, you can have a test.

You can modify the code like the attached code. I use the example for LPC5506 instead of LPC5516.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

3,426 Views
jmorel
Contributor II

in the end still didn't see any actions from the ACT portion ended up just following the IR and IE register as a status of the module.

0 Kudos
Reply