LPC5536 hard fault during clock config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5536 hard fault during clock config

ソリューションへジャンプ
1,654件の閲覧回数
WDA
Contributor I

About once in every twenty boots, I get a hard fault during clock config:

WDA_0-1668201917746.png

If I insert a delay before the divider setup (commented out in the above picture), I don't get faults anymore. Has anyone seen this kind of problem before, or know what might cause it? This is on a custom board with a 24MHz crystal.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,626件の閲覧回数
WDA
Contributor I

After talking with some FAEs from Avnet, we discovered that the Config Tools do not generate the code to wait for the XO_READY bit. After adding this line in clock_config.c, it is working fine.

    CLOCK_SetupExtClocking(24000000U);                            /* Enable XTALHF clock */
    while(!(ANACTRL->XO32M_STATUS & ANACTRL_XO32M_STATUS_XO_READY_MASK)); /* Wait for XO ready */

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,633件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

That sound like a hardware issue I recommend reviewing the schematic from the EVK maybe the crystal is not initialization well, please review the app note in the crystal recommendations. Hardware Design Guidelines for LPC55(S)xx Microcontrollers (nxp.com)

Best regards,
Pavel

0 件の賞賛
返信
1,627件の閲覧回数
WDA
Contributor I

After talking with some FAEs from Avnet, we discovered that the Config Tools do not generate the code to wait for the XO_READY bit. After adding this line in clock_config.c, it is working fine.

    CLOCK_SetupExtClocking(24000000U);                            /* Enable XTALHF clock */
    while(!(ANACTRL->XO32M_STATUS & ANACTRL_XO32M_STATUS_XO_READY_MASK)); /* Wait for XO ready */

 

0 件の賞賛
返信