LPC5516 ADC Channels

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5516 ADC Channels

2,533件の閲覧回数
adrian_lavin
Contributor I

We are using the LPC5516JBD64 which has eight ADC channels defined and want to use seven of them. Three of the channels share IO with the SWD interface. We would like to use the SWD to program the device at build time but after that use the IO as ADC inputs, Is there a recommended circuit configuration to allow this without using jumpers?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,515件の閲覧回数
frank_m
Senior Contributor III

From personal experience, I would recommend to avoid such configurations. You only barter for trouble.

0 件の賞賛
返信

2,523件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 It seems no, using jumper is easy method.

0 件の賞賛
返信

2,484件の閲覧回数
adrian_lavin
Contributor I

As an alternate solution, what pins on the SWD are required for programming. Is the SWO pin required to program the LPC5516 over SWD interface? Is the SWCLK and SWDIO the only connections needed to program over the SWD?

0 件の賞賛
返信

2,464件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

If you do not use SWO tracing technology, this pin can not used as SWD interface.

SWCLK, SWDIo and GND are necessary.

About debug design, you can have a look at:

https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565 

 

BR

Alice

0 件の賞賛
返信