LPC5516 ADC Channels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5516 ADC Channels

2,503 Views
adrian_lavin
Contributor I

We are using the LPC5516JBD64 which has eight ADC channels defined and want to use seven of them. Three of the channels share IO with the SWD interface. We would like to use the SWD to program the device at build time but after that use the IO as ADC inputs, Is there a recommended circuit configuration to allow this without using jumpers?

Labels (1)
0 Kudos
Reply
4 Replies

2,485 Views
frank_m
Senior Contributor III

From personal experience, I would recommend to avoid such configurations. You only barter for trouble.

0 Kudos
Reply

2,493 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 It seems no, using jumper is easy method.

0 Kudos
Reply

2,454 Views
adrian_lavin
Contributor I

As an alternate solution, what pins on the SWD are required for programming. Is the SWO pin required to program the LPC5516 over SWD interface? Is the SWCLK and SWDIO the only connections needed to program over the SWD?

0 Kudos
Reply

2,434 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

If you do not use SWO tracing technology, this pin can not used as SWD interface.

SWCLK, SWDIo and GND are necessary.

About debug design, you can have a look at:

https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565 

 

BR

Alice

0 Kudos
Reply