LPC55 USB host dual instance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55 USB host dual instance

3,736 Views
Michael_25
Contributor I

Dear,

We're actually working on a project using the two USB ports (HS/FS) of an LPC55S28 as host controllers.

When configuring both ports as host in MCUXpresso IDE, we get a message telling that only one host instance is allowed.

Could you please confirm there is no way to use the two ports as host with this USB library?

If yes, do you know any other USB stack capable to managing this configuration?

Thanks a lot,

Michael

Labels (2)
0 Kudos
Reply
2 Replies

3,723 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Michael,

Currently, it is a limitation of the USB component to support one more instance of USB device. 

We are not able to provide the update of the USB component to support two USB devices in the MCUXpresso Config Tools at the moment  due to limited capacity.

The only possible workaround is complete renaming of a generated USB code example (all files, global function and definitions) and generating a new one for the second USB device of the MCU. The shared definitions and USB device configuration must be merged.

Hope this helps,

Jun Zhang

0 Kudos
Reply

3,372 Views
dav1
Contributor V

any news on 2x usb's running at the same time, i.e one host one device?

0 Kudos
Reply