LPC546xx power lib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC546xx power lib

2,202 Views
chrisf
Contributor I

Hi,
we are in the process of migrating several projects to LPC546xx devices. Most of those projects do not use short enum/wchar compile options and are therefore not compatible with the compile settings of the provided power lib for Keil.

Can you please provide us with a version compiled without the short enum/wchar option, or is it possible to circumvent using this library?

 

Labels (1)
0 Kudos
Reply
3 Replies

2,193 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI chrisf 

LPC55 has keil_lib_power_disable_short_enum_wchar.lib but LPC546xx doesn't have the same. I will escalate it as feature request if necessary. but so far we don't have it.

Have a nice day,

Jun Zhang

0 Kudos
Reply

2,186 Views
chrisf
Contributor I

Hello Jun,

Thank you for your response.
We would really appreciate if you could escalate the request and provide us with a library. Changing all connected projects and libraries would probably add weeks or even months to the otherwise relative short task of replacing a BSP. I'd also need to check if all 3rd party libraries are available with this settings.

Chris

0 Kudos
Reply

2,178 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Chris

I got it. Thanks.

Best Regards

Jun Zhang

0 Kudos
Reply