LPC546xx footprint wrong pin-order

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC546xx footprint wrong pin-order

1,209 Views
tijmen
Contributor I

Dear all,

I'm using KiCAD to create a PCB with a LPC54618 microcontroller. I've downloaded the LPC546xxJxxxET180.bxl, the 180 ball BGA package, and used ultralibrarian.com to convert this file to KiCAD readable files.

The footprint in this converted file labels the pinrows on F.CU from left to right (FLTR) A14-A1, B14-B1 etc. while the datasheet LPC546xx.pdf page 11 mentions that the pins are labeled in transparent top view FLTR A1-A14, B1-B14 etc. Which of the 2 is correct? I am guessing the datasheet.

Is there something I forget?

Thanks in advance for your reply,

Regards,

Tijmen

Labels (1)
0 Kudos
Reply
1 Reply

1,166 Views
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
The datasheet is correct.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply