LPC54608 eva board ISP,SDRAM pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54608 eva board ISP,SDRAM pin

1,325 次查看
実奥山
Contributor II

CPU packege is 180-pin, TFBGA  in OM13092 board

C8 pin is connected to SDRAM and ISP switch.

There is a 2.2K resistor(R108) between the ISP switch and the CPU.

Why are you using a 2.2K resistor?

Shouldn't it be a 0 ohm resistor?

标签 (1)
0 项奖励
回复
1 回复

1,220 次查看
carstengroen
Senior Contributor II

My guess would be to protect the CPU if the ISP switch is pressed while the pin is used for accessing SDRAM. The 2.2K resistor will limit the current if switch is pressed during SDRAM access, at the same time its value is low enough to pull the pin low during boot (and activate ISP)