LPC54608 RS485 example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 RS485 example

3,291件の閲覧回数
rolandhösch
Contributor I

Is there any example out there who to configure a flexcomm USART port of the LPC54608 for serial RS485 communication?

ラベル(1)
タグ(1)
2 返答(返信)

2,274件の閲覧回数
primate
Contributor III

Opening the thread again since I am planning to get the LPCXpresso54628 Development Board but I am not sure how to implement the RS485 protocol entierly.

Also, I found an example RS485 and I presume the code can be modified to fit into the LPCXpresso54628 

Two LPC1765 devices communicating through RS-485? 

Thank for any help.

0 件の賞賛
返信

2,274件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

We only have the SDK for LPC54608 examples.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信