LPC54605J256BD100 microcontroller EEPROM Specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54605J256BD100 microcontroller EEPROM Specification

1,994 Views
prasannanaik
Contributor III

Hi,

   In LPC546xx datasheet, it is mentioned that upto 16 KB EEPROM is available but i couldn't find the exact details of the parts containing the EEPROM. I want to know whether LPC54605J256BD100 has EEPROM and if yes then please mention the size of EEPROM as well. Also, if LPC54605J256BD100 doesn't contain EEPROM then please suggest any  alternative part with 256KB flash,136 KB ram in LQFP package from LPC546xx family with EEPROM.

Thanks and best regards,

Prasanna

Labels (1)
0 Kudos
Reply
3 Replies

1,841 Views
prasannanaik
Contributor III

Thanks Sol. Do you have any document mentioning the size?

Best regards,

Prasanna

0 Kudos
Reply

1,841 Views
soledad
NXP Employee
NXP Employee

You can find this information in the user manual of this device.

https://www.nxp.com/docs/en/user-guide/UM10912.pdf   Page 47. 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,841 Views
soledad
NXP Employee
NXP Employee

Hi,

The EEPROM is available on all LPC546xx devices.

The EEPROM can be read and written/erased. A write operation involves two steps. The first step is writing a minimum of 1 word (4 bytes) to a maximum of 32 words (128 bytes) to the desired page in the 16 kB EEPROM address space at address 0x4010 8000. Step two is an erase/program of that page into non-volatile memory. There are 128 pages within the 16 kB EEPROM address space. The last page contains the EEPROM initialization data and is not writable. Note that data written to a page cannot be read back from the page address until the data have been programmed into non-volatile memory.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------