LPC54114: SPI_SCK line no CLOCK output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54114: SPI_SCK line no CLOCK output

1,641件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Guochd on Sun Jun 05 03:12:01 MST 2016
Hi,    
   Recently, I am debugging SPI master demo program  on LPCxpresso54114 Evaluation board OM13089. But I found that SPI clock line no clock output.
It is strange that SPI clock line is changed with the mode sate changed in (mode0 to mode3), and SPI data line also is changed with the TX buffer's last bit.
NO clock ,I did't understand , anybody can help me  :quest:
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,510件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,510件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Hi Gouchd,

Are you using an LPCOpen example? Please provide more details...

0 件の賞賛
返信