LPC54114: SPI_SCK line no CLOCK output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54114: SPI_SCK line no CLOCK output

1,652 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Guochd on Sun Jun 05 03:12:01 MST 2016
Hi,    
   Recently, I am debugging SPI master demo program  on LPCxpresso54114 Evaluation board OM13089. But I found that SPI clock line no clock output.
It is strange that SPI clock line is changed with the mode sate changed in (mode0 to mode3), and SPI data line also is changed with the TX buffer's last bit.
NO clock ,I did't understand , anybody can help me  :quest:
Labels (1)
0 Kudos
Reply
2 Replies

1,521 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,521 Views
brendonslade
NXP TechSupport
NXP TechSupport

Hi Gouchd,

Are you using an LPCOpen example? Please provide more details...

0 Kudos
Reply