LPC5410 SPI Master with DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5410 SPI Master with DMA

1,717 Views
genisaguilar
Contributor II

I am having some trouble at using SPI as Master with DMA transfers enabled in an LPC5410. I couldn't find any good reference code so I'm basing mine on the one in the current version of LPCOpen, which has SPI+DMA though acting as slave.

Does anyone know any reference code I could look at?

Tags (2)
0 Kudos
Reply
1 Reply

1,489 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Genis,

There is another example of SPI slave with DMA that you can also use as reference, it can be found on the LPCOpen package for the LPCXpresso LPC54102 Sensor Processing/Motion Solution Boards:

LPCOpen Software for LPC5410X|NXP 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply