LPC54018 I2s Config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54018 I2s Config

4,171件の閲覧回数
Sukumar_M
Contributor I

Hi,

I'm newly working on I2s I should try to do demo driver flash to evk but it not work how can achieve configration. please any one help me.

0 件の賞賛
返信
7 返答(返信)

4,154件の閲覧回数
Sukumar_M
Contributor I

i2s interrupt transfer demo if any other option to use polling method

0 件の賞賛
返信

4,146件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sukumar_M,

I test the I2S demo on my side, it can works well. So recommend you first do not change anything with demo.

 

BR

Alice

0 件の賞賛
返信

4,144件の閲覧回数
Sukumar_M
Contributor I

ok how to choose frequency divider value as per music. I can choose same frequency divider value multiple music is it possible

0 件の賞賛
返信

4,112件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

About I2S sample rate configuration, you can refer to:

UM11060 -> 29.8.3.2 Rate calculations  

 

0 件の賞賛
返信

4,159件の閲覧回数
Sukumar_M
Contributor I

already one demo are there in MCUxpresso but it not work only noise are occur no sound data should be transfer.

0 件の賞賛
返信

4,157件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Which demo you used? Have you configure well refer to readme? Do you use DEMO board from NXP? 

 

BR

Alice

タグ(1)
0 件の賞賛
返信

4,165件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Recommend download SDK , there is I2s demo, and there is  readme.txt under project folder about how to use demo:

https://mcuxpresso.nxp.com/en/builder?hw=LPCXpresso54018  

 

 

BR

Alice

0 件の賞賛
返信