LPC54018 ADC accuracy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54018 ADC accuracy

1,279件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Hello,

We test SDK_2.5.0_LPCXpresso54018\boards\lpcxpresso54018\driver_examples\adc\lpc_adc_basic\iar example for 

LPCXpresso540xx Eval Brd Rev E. We get below result:

3.253v for Power on LPC54608 VDD pin VDD_TARGET_IC.

When input 0.156v actual value voltage, get adcResultInfoStruct.result 192 on channel 4, theoretical value is 0.152v=(3.253/4096 X 192), error is 0.004v =(0.156v-0.152v). 

When input 1.650v actual value voltage, get adcResultInfoStruct.result 2048 on channel 4, theoretical value is 1.6265v. 

error is 0.0235v.

When input 1.488v actual value voltage, get adcResultInfoStruct.result 1856 on channel 4, theoretical value is 1.474v.

Error is 0.014v. 

When input 3.253v actual value voltage, get adcResultInfoStruct.result 4093 on channel 4, theoretical value is 3.2506v. 

Error is 0.0024v.

We want to know why error could up to three digits after the decimal point when close to 0v or close to Vdd voltage,

but only two digits after the decimal point from 1v to 2v voltage. 

Do you have some improve method for this?

ラベル(2)
0 件の賞賛
返信
1 返信

1,147件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Hanson,

Sorry for the delay.

I have contacted AE team, they said they had tested the ADC performance and answered your question.

BR

XiangJun Rong

0 件の賞賛
返信