LPC51u68 lpcxpresso51u68_dev_cdc_vcom_bm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC51u68 lpcxpresso51u68_dev_cdc_vcom_bm

2,231件の閲覧回数
filipecostapica
Contributor I

Hello to everyone.

I'm running the SDK example "lpcxpresso51u68_dev_cdc_vcom_bm" on a controller(LPC51U68JBD48E) placed on my customized board.

It is expected to: "The Virtual COM project is enumerated as a COM port, which the users can open using terminal tools, such as TeraTerm. The demo echoes back any character it receives". 
I followed the user manual to connect the USB:
pastedImage_3.png

and the USB works fine. i.e- PC detects a COM port when I plug the USB to the PC.
pastedImage_4.png

But when I try to communicate trough teraTerm nothing happens so I doubt the communication is working. What am I doing wrong? Is this a windows problem? 


All the best,
Filipe Costa

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,101件の閲覧回数
filipecostapica
Contributor I

Hi jeremyzhou‌,

I haven't found your attach. Can you please resend it?

Sure I can.

pastedImage_3.png

BLOCO_USB:
pastedImage_4.png


Have a great day,

Filipe Costa

0 件の賞賛
返信

2,101件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Filipe Costa,
The USB interface seems good, and please check the attached tool.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,101件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Filipe Costa,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I've attached a tool which is able to observe the enumeration process of a new attached USB device, please use it to validate the USB CDC device enumerate successfully.
In further, I was wondering if you can share the schematic of the USB interface of your customized board for me to check.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信