LPC51U68 reference history, information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC51U68 reference history, information

2,422 Views
zhaoyunlong_164
Contributor I

Hi:

      I am going to use the LPC51U68 development project but I can't find a related reference design and hope to get some help.

      1.Routine

      2.IAP development materials

      3.How to get the MCU ID?

      Thank you.

Labels (1)
0 Kudos
Reply
4 Replies

2,217 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello 云龙 赵 ,

Have you still have question after refer to Con Verse' answer ?

BR

Alice

0 Kudos
Reply

2,217 Views
zhaoyunlong_164
Contributor I

Hi Alice

   Is there any detailed development tutorial and program for IAP? Because I have not developed it before, so I may not know how to start. What should I pay attention to?  

   Thanks.

0 Kudos
Reply

2,217 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

- I recommend you first can have a look at the demos under SDK package, it also includes IAP program "flashiap", download from:

https://mcuxpresso.nxp.com/en/select    

pastedImage_2.png

- About hardware development , there is a demo board LPCXpresso51u68, you can refer to the schematic:

LPCXpresso51U68 board for LPC51U68 MCU | NXP      

- About MCU ID, do you mean UID? If yes, please refer to this thread:

LPC51U68 Read UID 

Hope it helps,

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,217 Views
converse
Senior Contributor V

You can find this information in the User Manual, which can be found on the Documentation tab of this page: LPC51U68 | NXP 

0 Kudos
Reply