LPC51U68 min USB VDD 3V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC51U68 min USB VDD 3V

1,418 Views
jh0
Contributor IV

Hi,

Is there any way to use LPC51U68 USB with 1.8V VDD. If not, is there any similar device (M0+ 100MHz) with this possibility.

Labels (1)
0 Kudos
Reply
2 Replies

1,321 Views
soledad
NXP Employee
NXP Employee

Yes, the LPC51U68 it is one self-power supply, as you can review in the datasheet of the device Section 13.6 Suggested USB Interface Solutions.

Best Regards,

TIC Support Team

0 Kudos
Reply

1,321 Views
jh0
Contributor IV

In Section 13.6 fig 33 VBUS(1) is combination that I want. Question is if in case of VDD=1.8V USB (CDC device) can work or not? Because in table 12 (10.1 General operating conditions) there is min 3.0V VDD specified for USB operation only!

0 Kudos
Reply