LPC51U68 min USB VDD 3V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC51U68 min USB VDD 3V

1,411件の閲覧回数
jh0
Contributor IV

Hi,

Is there any way to use LPC51U68 USB with 1.8V VDD. If not, is there any similar device (M0+ 100MHz) with this possibility.

ラベル(1)
  • USB

0 件の賞賛
返信
2 返答(返信)

1,314件の閲覧回数
soledad
NXP Employee
NXP Employee

Yes, the LPC51U68 it is one self-power supply, as you can review in the datasheet of the device Section 13.6 Suggested USB Interface Solutions.

Best Regards,

TIC Support Team

0 件の賞賛
返信

1,314件の閲覧回数
jh0
Contributor IV

In Section 13.6 fig 33 VBUS(1) is combination that I want. Question is if in case of VDD=1.8V USB (CDC device) can work or not? Because in table 12 (10.1 General operating conditions) there is min 3.0V VDD specified for USB operation only!

0 件の賞賛
返信