LPC45628 Errata 3.22

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC45628 Errata 3.22

4,557 Views
samuelguido
Contributor II

I'm reposting this the last thread seems to be closed. I'm in desperate need of a solution to this issue and the latest SDK (2.9.0) doesn't seem to address this errata.

Please HELP!

Sam Guido

 

3.22 USB.15: USB high-speed device in endpoint TX data corruption

samuelguido_0-1616454088894.png

 

My question is, how can the application programmer ensure that the required NAK is generated?

For example, if I already have data queued to send to the host (Tx IN), as would normally be the case for USB, then how can in interrupt this transfer and insert an NAK?

 

Or is this handled in the SDK?

(I'm using SDK 2.5.0)

Any clarification would be much appreciated.

0 Kudos
Reply
5 Replies

4,537 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @samuelguido,

I will contact you directly regarding this issue.

Best Regards,

Alexis Andalon

0 Kudos
Reply

4,423 Views
andyjackson
Contributor III

I'd like to know how to address this issue as well...

0 Kudos
Reply

4,414 Views
samuelguido
Contributor II

Andy,

This problem occurs if USB length % 8 = 4. If the USB packet length satisfies this test, then the USB packet is broken up in to 2 USB packets where the 1st is the length/2-1 and second is length-(length/2-1). These 2 packets will be sent instead of the original packet. This ensures that neither USB packet will satisfy the condition.

I handled it at the lower levels of my host code like this (java):

ArrayList<ByteArray> dataList = new ArrayList<>();

if((data.getIndex() % == 4)
{
byte[] halfData = data.readArrayBytes();
int ba1_size = (halfData.length / 2) - 1;
int ba2_size = halfData.length - ba1_size;
ByteArray ba1 = new ByteArray(ba1_size, ENDIAN.BIG);
System.arraycopy(halfData, 0, ba1.getBytes(), 0, ba1_size);
ba1.setIndex(ba1_size);
ByteArray ba2 = new ByteArray(ba2_size, ENDIAN.BIG);
System.arraycopy(halfData, ba1_size, ba2.getBytes(), 0, ba2_size);
ba2.setIndex(ba2_size);
dataList.add(ba1);
dataList.add(ba2);
}
else
{
dataList.add(data);
}

Hope this helps.

 

Sam...

0 Kudos
Reply

4,400 Views
andyjackson
Contributor III

Hello Sam,

Thank you for your reply and I have implemented similar mitigation code in the host app but unfortunately it will only work reliably on Windows when the Out data rates are low. Once the data rate increases the Windows driver doesn't have to respect the data boundaries of the application and is at liberty to concatenate data in order to achieve the best overall system performance which can result in USB Out packets that can trigger the error condition.

Ultimately I think that without the ability to change the host driver code the only option to resolve this errata is to handle it at the device end. However as yet I've not seen anything from NXP detailing how this can be achieved which is surprising at it appears to affect at least the LPC546xx (errata USB.15) and LPC540xx (errata USB.3) families.

Andy

0 Kudos
Reply

4,522 Views
BenDev
Contributor II

Hi @Alexis_A ,

Can you please contact me directly regarding this issue too as I'd like to know if there is a solution. I can currently replicate the Errata 3.22 issue with a simple example using the latest SDK and a python script to verify the integrity.

Regards,

Ben

0 Kudos
Reply