LPC43xx sd/mmc card acquire fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43xx sd/mmc card acquire fails

1,475件の閲覧回数
rickrigby
Contributor II

LPC43S57 MCU, using SD/MMC driver (CIU). SD_CMD signal phase is opposite that needed by my card. Is there any way to change the 'phase' of the SD_CMD/SD_DATn signals so they are valid on the rising edge of SD_CLK instead of being valid on the falling edge of SD_CLK during card acquire? (CMD0, CMD1, CMD2).

I'm running the sd/mmc example code from LPC43xx examples.

Windows, Linux, and OSX hosts all use 'phase 0', data valid on rising edge of SD_CLK. Why is the LPC43S57 SD/MMC host opposite?

ラベル(3)
0 件の賞賛
返信
1 返信

1,309件の閲覧回数
Dezheng_Tang
NXP Employee
NXP Employee

I see some discussion on this but didn't try myself:

https://www.lpcware.com/zh-hans/node/1110550

0 件の賞賛
返信