LPC43xx USB isochronous mode & windows driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC43xx USB isochronous mode & windows driver

1,149 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RichardsonM on Fri Jul 06 04:02:13 MST 2012
Hi,

I'm looking at using an LPC43xx device with the USB port running in isochrounous mode using nxpUSBlib for a high speed custom data interface (up to around 150Mbps). Is this possible and do you know if there's a windows driver that I can use from a custom windows application to access the data sent from the LPC43xx?

Thanks for any help you can provide.
标签 (1)
0 项奖励
回复
0 回复数