LPC43xx LPC4333 LPC4337 USB0_VDDA3V3 not connected on PCB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43xx LPC4333 LPC4337 USB0_VDDA3V3 not connected on PCB

1,730件の閲覧回数
jueboe
Contributor I

I have a PCB for LPC4333 still now without parts. I don't need the USB modules. On this PCB are the pins USB0_VDDA3V3 and USB0_VDDA3V3_DRIVER not connected to power 3.3V (floating). It is possible, that this PCB work without the connections on this pins?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,716件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

If they are unused, Please tie these two pins to VDD.

Hope this helps,

Jun Zhang

0 件の賞賛
返信

1,710件の閲覧回数
jueboe
Contributor I

Thanks! 

What will happen without the connections of the pins USB0_VDDA3V3 and USB0_VDDA3V3_DRIVER to VDD?

(I cannot connect the two pins on my PCB (LBGA with 256 pins). I can only let produce new PCBs.)

 

0 件の賞賛
返信

1,701件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi jueboe,

We suggest you defining unused pins as our recommendation.

There is no full report if you use it in another way. So I can't say what will happen as this is not our recommended way of using . If so, we can't guarantee chip work normal, working like this for long time may potentially reduce part life

 

Have a nice day,

Jun Zhang

0 件の賞賛
返信