LPC43xx Deep power down wakeup after more than 64seconds

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43xx Deep power down wakeup after more than 64seconds

1,969件の閲覧回数
KhaVo
Contributor I

Hi all,

As LPCOpen sample pmc_states.c,

        Chip_ATIMER_DeInit(LPC_ATIMER);
        ATIMER_ClearInts();
        Chip_ATIMER_Init(LPC_ATIMER, RTC_ALARM_TIME*1000);
        LPC_ATIMER->DOWNCOUNTER = RTC_ALARM_TIME*1000;
        Chip_ATIMER_IntEnable(LPC_ATIMER);
                
        /* Call Pre SleepPowerDown function */
        PMC_Pre_SleepPowerDown();

        /* Goto Deep Sleep mode */
        Chip_PMC_Set_PwrState(Pwr_state);

MCU will wake-up by ATimer, but this is Timer 16bit and runs at 1024Hz clock, so the maximum time is 64 second.

1. How could sleep more than that?
2. Is RTC wake-up really work? If it is, why we need to config the ATimer?


Thanks in advance!


Regards,
Kha Vo

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,674件の閲覧回数
KhaVo
Contributor I

Hi jeremyzhou,

Thanks for your answers!

So to sleep longer, I need to use RTC wake up. I face another problem with RTC initializing that it take 2 second to init RTC each booting. I've posted this issue here.

Hoping that you or others could help!

Thanks,

Kha Vo

0 件の賞賛
返信

1,674件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Kha Vo,

1. How could sleep more than that?

The maximum period is 64s, as the counter/timer clock is fixed :1024 Hz.

2. Is RTC wake-up really work? If it is, why we need to config the ATimer?

In my opinion, the Atimer is particular to generate periodic interrupt which can be used to wake up the device from a low power mode, however the RTC is more complicated than it.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信