LPC4367 MCU getting locked

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4367 MCU getting locked

1,280 Views
manish_sharma2
Contributor II

Dear Sir,

 

we are using LPC4367 MCU in our design. It was observed that the MCU was getting locked and we need to erase it again to work on it.

 

While comparing with the reference schematic LPCXpresso43/18xx v3 Rev B, we found that the pin connected to JTAG programming is having different pullups.

IF_TDO_SWO: 100K pullup

IF_TMS_SWDIO: 100K pull up

IF_RST: 100K pull up

TCK-SWDCLK_TRGT: 2.2K pullup

IF_JTAG_TDI: No pull up

 

In my design we have used fixed 10K pull up. Can you please explain why different pullup are needed and what is the use of NX3DV2567GU,115 Analog switch.

Thanks

Manish Sharma

 

0 Kudos
Reply
1 Reply

1,271 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Manish Sharma,

Please follow this design considerations for your JTAG design.

https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44

 

WHy you wonder your MCU locking is due to Jtag design?

 

Have a nice day,

Jun Zhang

 

0 Kudos
Reply